Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Excited to see a new connector on new STM32 Nucleo 144 boards like the Nucleo-H5E5ZJ. Is the Connector intended for customers to design their own modules only, or will ST offer a module as well? PS: I still hope to also see a Qwiic connector, or at...
I am currently using the NUCLEO-H563ZI board to test SPI functionality. I configured SPI1 as a master and was able to successfully transmit and receive data using HAL_SPI_TransmitReceive(). However, when I switched to SPI2, I found that the clock sig...
Hello!I just bought the stlink-v3minie for myself but I am unable to flash my board using it. I can program my board with a borrowed stlink-v3pwr but not with the minie.I have upgraded the firmware on it and it still doesnt work. It fails with this o...
Reference Board: Nucleo-H753ZI (MB1364, ST-LINK V3, rev B) Summary We have an external UART sensor (WitMotion HWT9053 IMU) connected to the Arduino D0/D1 header pins on a Nucleo-H753ZI. The sensor is confirmed working on Arduino. We have veri...
I realized that in my discovery board with STM32F411VE the accelerometer/magntometer is lsm303agr and not lsms303DLHC. I would have an updated schematic.
quectel bg96 does not reply to messages from stm32l496ag on kit board p-l496g-cell02 but since I bought it. I could not even start blink the led on bg96 so I assume there is something missing to me. I use usb cable to stlink com and debug from the so...
Hi, I am using the STM32L4 B-L475E-IOT01A board with Wi-Fi module Inventek system ISM43362-M3G-L44.I have seen the example WiFi projects but they do not have the .ioc file. So my question is, is there any middleware available in STM32CubeMX which can...
I am experiencing issues powering the STM32H755ZIT6 MCU on our custom board. The schematic has been derived from the NUCLEO-H755ZI-Q development board reference design, and we have verified that there are no apparent design or assembly errors. Howeve...
Hi, I'm a beginner programming a NUCLEO-N657X0-Q. The LD5 is blinking and I can't get a connection to the board. Even with the demonstration code/project, it wouldn't work. In STM32CubeIDE I get the attached error message. As of yet, I never got to...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.