Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Split from Benchmark Validation in App does not match Arduino Uno R4 WiFi as this is a new question.thanks for the response @Andrew Neil If i'm not overstepping my bounds, given the requirements of an audio classifier (also need wifi support and disp...
Hello, I read somewhere that I can use the ST-LINK built into my H563ZI to program my custom cards with STM32F401.Could someone help me figure out how to do this?Thanks in advance.
Hello everyone, I'm facing a very frustrating issue with USART2 on my Nucleo-L475VGT6 board using the built-in ST-LINK Virtual COM Port. What works: - ST-LINK is detected (COM3 appears, Windows sound plays on connect) - Code downloads successfully (n...
iam attatching a pdf of my ki cad , let me know the what prevents to flash my code . this is the below error message coming while iam trying to flash " Starting server with the following options: Persistent Mode : Disabled Logging Level : 1 Listen Po...
Hello ST Community,I’m using an STLINK-V3MINIE and I’m trying to fully understand the hardware on the probe PCB.On the bottom side of the STLINK-V3MINIE PCB there is an unpopulated footprint labeled “CN5” (small pad footprint). I could not find any m...
Hi everyone, I recently bought an EVSPIN32F0602S1 board, but I’m unable to connect to it. Windows is giving me an error when I plug it in. I’ve already tried changing the USB cables and even tested it on different laptops, but I’m still gettin...
Hello,I am currently using the X-NUCLEO-53L7A1 expansion board together with the NUCLEO-F401RE development board.I would like to add a Bluetooth module (HC-05 or HC-06) to this setup in order to transmit measurement data wirelessly.Could someone plea...
we are facing after migrating our design from STM32F405ZGT7 to STM32H743ZI.We have an automotive application where a horn load creates significant EMI transients. With our previous design using STM32F405ZGT7, the system was stable and did not experie...
I noticed two holes at Bottom of the MCU area on the STM32G4 Nucleo board. What is their purpose?
HelloI'am new to STM32 and i want to create project that interface with user using uart with serial monitori configured usart and used hal_uart tarsnmit function but it didnt work when the tutorial im following worked for himwhat can be the issue?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.