2026-02-28 3:05 AM
Hello!
I just bought the stlink-v3minie for myself but I am unable to flash my board using it.
I can program my board with a borrowed stlink-v3pwr but not with the minie.
I have upgraded the firmware on it and it still doesnt work. It fails with this output:
ST-LINK SN : 003300313235510537333439
ST-LINK FW : V3J17M10
Board : STLINK-V3MINIE
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x451
Revision ID : Rev Z
Device name : STM32F76x/STM32F77x
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x93
Opening and parsing file: ST-LINK_GDB_server_a28496.srec
Memory Programming ...
File : ST-LINK_GDB_server_a28496.srec
Size : 668.68 KB
Address : 0x08000000
Erasing memory corresponding to sector 0:
Erasing internal memory sectors [0 6]
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.18.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.100.202412061334\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
Does anyone have any ideas on how to fix it or what I am doing wrong.
Thanks in advance!
Solved! Go to Solution.
2026-03-01 10:01 AM
Ok turns out after updating all software it works now. My bad:grinning_face_with_sweat:
2026-02-28 6:36 AM - edited 2026-02-28 6:39 AM
Hi,
try connect with CubeProgrammer , set: hot plug, soft. reset ;
connect ...?
- check: write protection : not set (on all sectors)
- do a full chip erase
- try: flash your prog
2026-03-01 5:37 AM
Hi!
Thanks for the response!
I can connect via CubeProgrammer. I can also see that Write protection is not enabled on any sector. I did an erase but I am still unable to flash with the stlink-v3minie. If I use the stlink-v3pwr I can flash the chip.
Any other advice i greatly appreciated!
2026-03-01 6:16 AM
(This cannot be...!)
So how the target gets power ? stlink-v3pwr ? and using miniE ?
+
Connect with CubeProgrammer, try to read and write some data from/to flash in the HEX view / edit window.
set: hot plug, soft. reset ; try same.
Is connection to target stable if just let it be connected 10 mins or so ?
2026-03-01 6:47 AM
The power is from a buck converter on my board which gets its power from a usb cable. The power is stable. I can repeatably progam my board using the stlink-v3pwr through the STDC14 cable. but when i swap it to the stlink-v3minie then it fails. I even tried different cables.
To prove that its not power related, I now connected 3.3V directly from a lab psu.
Now when trying to make a screenshot showing that i can indeed edit memory with the minie I discovered that it sometimes works and sometimes doesnt.
Could it be that I got a faulty stlink? (I doubt that)
Thanks for the response.
2026-03-01 7:47 AM
I use a V3mods here and some V2-"sticks" , at work most time a miniE ; all working fine.
Why i asked about supply and connections: i found the V3 much more sensitive to spikes or stray in, even the ground connection is critical, than old V2 versions. (Or i just got a super "sensible" device here.)
Problems then : debug not working, or only some seconds, etc.
I had the supply for target plugged to mains at wall and PC is on another - didnt work in useful way.
But when cables close together and target gets power from same power strip as PC - working fine.
So your >that it sometimes works and sometimes doesnt. < could come from ground/stray in.
Play a little with connections, where its plugged in , etc.
2026-03-01 10:01 AM
Ok turns out after updating all software it works now. My bad:grinning_face_with_sweat:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.