Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Can somebody tell me whether I am, or not, powering this STM32H725RG in the right way?As far as I know, after reading several times the specs, the 68 pin package doesn't have LDO (SMPS only).I've built my first board this way and the MCU got burnt. ...
Hello everyone, I am new to STM32 and recently purchased the STM32 NUCLEO‑F446RE development board to start learning microcontrollers. While studying the clock configuration, I saw the option to use HSE (High Speed External oscillator). Since I am a ...
Hello,I have ordered a X-NUCLEO-PLC01A1 for my Nucleo Board F767Zi.I should receive it soon but I would like to understand it as much as possible.This is why I try to find some example projects but I cannot find any.In addition, I have tried to downl...
Hello everyone,I've been working on getting Ethernet working on the STM32H750B-DK discovery board with TouchGFX and LwIP. After extensive debugging, I suspect a hardware issue and would appreciate your advice on confirming this.What Works ✓TouchGFX d...
Dear ST team,I am planning to use STM32H753ZIT6 in my design and also planning to use NUCLEO 144 H7 LEGACY for development activities. Could anyone help me whether I can use the NUCLEO 144 H7 LEGACY board to program the STM MCU which is going to asse...
This is to NUCLEO-H723ZG/NUH723ZG$AT2 eval board. When set VDD=3.3V by JP5, the ethernet (lwip + no os) DHCP is working fine and stable. When switch to VDD=1.8V by JP5, the STM32 is working fine but the ethernet DHCP is working randomly, most of time...
Hello, I have a board STM32F746G-DISCO from Farnell and I noticed that stm32cubeprogrammer is not showing the correct target board information. I have tried different version of stm32cubeprogrammer using different PC (2.15.0 due to usage of Windows...
Hi,I wanted to use an external voltage reference of +2.048V on the Nucleo Board. To do so I removed SB57 as dictated in UM1724 document: SB57 (VDDA/VREF+)ON VDDA/VREF+ on STM32 is connected to VDD.OFF VDDA/VREF+ on STM32 is not connected to VDD and c...
Hello everyoneI am using a Nucleo H7S3L8 evaluation module am I am trying to get some GPIOs and peripherals to work. I have generated a demo project that toggles a few LEDs and that works. Then I started replacing the GPIO ports (A, B, etc.) and pin ...
Dear STMicroelectronics Community,I am experiencing a critical issue with my NUCLEO-144 STM32N657X0 EVAL BRD following an attempted ST-LINK firmware upgrade.During the ST-LINK upgrade process (via STM32CubeProgrammer), the upgrade became stuck and di...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.