Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
hello, could you please tell me where the default jumper wires be placed on the board h743zi2. quick response is much appreciated as i am in a hurry with the deadline. pictures of the board are much needed while answering.
Hello, I generated a project for STM32U5A9J-DK with STM32CubeIDE (v1.16.0). It doesn’t include the OctalFlash test code. So, I used the test codes in chapter "Octo-SPI FLASH in Regular-command protocol example" of attached AN5050.The mounted OctalFla...
Hi there.I want to download my bin file to one of my customized board ( target STM32G030F6P6).The problem is the debugger pin CN1 of Hardware board MB1441 has 5V input but my one has 2.8 V in debug connector.Kindly recommend a solution for voltage le...
Hello,I am currently developing on an STM32H743. I have a bootloader and an application that I want to load into the internal flash memory of the microcontroller. The bootloader is written successfully, but the application fails to load.Instead of wr...
Hi,I have Nucleo-F767zi . When I give it an external power source through Vin. It doesn't always wake up. The board works if I reset it.The graphic of my power supply; It arrives 9V at 400 mili seconds. The curve is almost linear.(No glitch on the w...
When I connect my STM32F401RE board to the PC via USB cable, a FAIL.txt file appears with the message 'The interface firmware FAILED to reset/halt the target MCU.' I tried following the tutorial https://www.youtube.com/watch?v=Ib0KMuv6cxA&t=192s, bu...
HI, I want to implement the USB middleware on the STM32G0B1RCT6 to use the CDC class for opening a virtual COM port. Can someone provide an example driver?
Hello, Looking for a small size STM development board with USB and crypto functionality support
I'm using the i2c on a nucleo stm32h723 board. I'm using pins PB8 and PB9 on the board. I have the pins connected to a scope. I notice that when I have the internal pullups of the board on the voltage is at 3.5V and if I dont use the internal pullup,...
Hello,I have a new STEVAL-IDP004V2, and I recently downloaded both the ST-LINK Utility and the STM32CubeProgrammer. I'm going through AN5041 Rev 5, page 22 steps which mention the board is to be programmed with the ST-LINK Utility. I started trying ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.