2024-09-05 12:24 AM
Hi there.
I want to download my bin file to one of my customized board ( target STM32G030F6P6).
The problem is the debugger pin CN1 of Hardware board MB1441 has 5V input but my one has 2.8 V in debug connector.
Kindly recommend a solution for voltage level shifting.
And also share Hardware board MB1441 schematic.
BR
HASAN
2024-09-05 7:38 AM
CN1 of the STLINK-V3SET has CMOS 3.3V interfaces, not 5V.
The B-STLINK-VOLT board extension is a 1.65V-3.3V voltage adapter board for the STLINK-V3SET.
The entire toolset is not open source, so the schematics are not publicly available.
Hope that answers your questions?
Regards
/Peter
2024-09-05 9:24 AM
Peter,
Thank you for clarification.
Do you have CN1 pin map? Let me know. Figure out the location of 1.5 to 3.3v source.
2024-09-05 11:19 AM
You can find the pin map of CN1 in UM2448, section 8.2.1.
2024-09-12 2:52 AM
CN1 connector is not providing 3.3V.
I succed it when I put 3.3V externally.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.