2024-09-10 6:27 AM
Hello,
I have a new STEVAL-IDP004V2, and I recently downloaded both the ST-LINK Utility and the STM32CubeProgrammer. I'm going through AN5041 Rev 5, page 22 steps which mention the board is to be programmed with the ST-LINK Utility.
I started trying STM32CubeProgrammer as ST-LINK Utility is not recommended for new designs, but I kept getting read errors after the system was trying to program option bytes: "Error: Data read failed". The option bytes were set correctly, to AA=level 0.
I decided to try the ST-LINK Utility, set the option bytes to level 0, and no problem, no programming errors.
I then try to program with STM32CubeProgrammer, and after using ST-LINK, no problem, no programming errors.
What's the difference? Does STM32CubeProgrammer have a bug? Is it unable to set the option bytes?
My versions are:
STM32CubeProgrammer Win64 v2.17.0
STM32 ST-Link Utility v4.6.0
O/S: Windows 10 Pro
Programmer: ST-LINK/V2
Board: STEVAL-IDP004V2A, Trace code: XD109912, Bulk ID: Z1X099120047
Solved! Go to Solution.
2024-09-10 6:41 AM
I think I just solved my own problem.
I thought the option bytes was something I set in the option bytes window of STM32CubeProgrammer, then download the program, but it seems I needed to click the "Apply" button in the option bytes window!
No worries!
2024-09-10 6:41 AM
I think I just solved my own problem.
I thought the option bytes was something I set in the option bytes window of STM32CubeProgrammer, then download the program, but it seems I needed to click the "Apply" button in the option bytes window!
No worries!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.