Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi I have been seeing voltage spikes and drops on the signals coming from the ADC. I'm not sure what is happening and wanted to see if anyone else has seen this before.
Hi,Do you have any suggestions on how to start developing or integrating a third-party PROFINET stack on an STM32 evaluation or discovery board? I would like to create my own application for a PROFINET master and slave. If there are any example codes...
Hello, I am wanting to configure the SDIO peripheral on my STM32F407G-DISC1 to write a file to a 16GB type 10 micro SD memory. The problem is that I am receiving the FR_NOT_READY error when I want to create a file and I don't know what the problem is...
Hello,My STM32L452 Nucleo-64 board does not wake up from sleep mode by an external interrupt.Interrupts are working, but after calling this function: HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI); Program wait on this function ...
STM32F746G - will this MCU support for tone generation using PCM-PWM and PCM-TDM. Where i can get the refernece manual for this mcu.
Hi, I have a customized STM32G0B1RCT6 board, and I'm trying to use its USB host function to connect to a flash drive. I used the file handling function to create a text file and store text files from the controller to the USB. I tried the same steps ...
Hello, I am working on a project which receives an analog square signal and the idea is to read the ADC values, and try to recreate (based on the ADC values) the square signal inside the microcontroller, but not to output in another pin, instead to d...
So a bit off-topic, but arose in the context of STM32 Nucleo boards:https://community.st.com/t5/stm32-mcus-products/communication-between-nucleo-f411re-and-raspberry-pi-using-st/m-p/721571 "Virtual COM Port" is a Windows-centric term - referring to t...
I folloe the nucleo-h7s3l8 HID example to create my project (by STM32Cubemx), But it is not work.Pc always didnt detect ny board.I trace code to here(like the picture) when I use debug toolIn my code ,the CAD_StateMachine_SNK run onec time and _hand...
Hi, everyone.I cut the stlink board from my Nucleo-F722ZE board.And I supplied 5V power through E5V of CN11 And JP3 was set to E5V.I confirmed that the PWR LED was on.But the embedded program did not run.I confirmed that this Nucleo-F722ZE board rece...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.