Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello ST Micro community,I'm working with a NUCLEO-F746ZG board and have noticed some interesting behavior regarding memory usage. I'd like to seek your advice on the following:The VTOR (Vector Table Offset Register) is currently set to 0x00200000.Th...
Hi,I recently got a STLINK V3 SET and wondered if I could get some help setting it up to work with a board similar to the SMARTAG1. (I created a custom PCB with a very similar layout)I was trying to follow this post: https://community.st.com/t5/stm32...
I am having trouble with my new board , in device manager I see my board as undefined USB device and error code number:10 after downgrade onboard STlink I have this issue (current version: stlink-V2.J21.S4.).Not all STM32 drivers are installed becau...
Hello everyone, I have had problems flashing a STM32F405 from a 3D printer board, I have not managed to flash via DFU and with a STLink-V2. Here is what I have done. - First, the board has a HID bootloader, which by connecting jumpers between BOOT0-3...
Hello, I have been using the same cubeIDE debugger options for several months and have not had any major issues. However i recently updated to the latest macOS 15.0 release (not necessarily the cause, but it's the only change that comes to mind) and ...
I didn't own a V3 programming device and found the $11 device did have a USB C type connector but would not supply power to the target so I purchased the STLINK-V3PWR device. When it arrive I could not find any of the shipped cables that would connec...
In my program, I implemented a sleep using the STOP2_Mode, and to wake the MCU again, I have to depend on interrupts and events. I have attached the image of the block of code which represents the STOP mode mechanism. When the device gets in STOP mod...
Hi, it's my first time using a STM32-NUCLEO-F411RE (actually the STM32 in general) and im trying to get some audio using a i2s MEMS microphone, modifying it using the DSP, and outputting it on another i2s.The microphone is working, and im turning a l...
Hello everyone I would like to ask about a warning on my STM32 hardware. I'm using an STM32F405 board that I designed myself. I use NUCLEOf334 as the debugger (ST_LINK). I make sure that I have removed all the jumpers on the nucleo so as not to inter...
NUCLEO STM32 I2CHello, I'm trying to make a master NUCLEO-FR103RB send data to a slave device using fast mode (400 kHz). Slave to master is not essential at the moment. As slave I am using the Total Phase AARDVARK in slave mode simulating a LED drive...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.