2025-12-11 3:41 PM - last edited on 2025-12-12 2:03 AM by Andrew Neil
Regarding the STPS5H100AF, the datasheet states that the storage temperature is -65 to 175°C, but there is no mention of the operating temperature.
What is the operating temperature?
2025-12-11 11:46 PM - edited 2025-12-11 11:51 PM
Well, in addition to the storage temperature range, the data sheet of the STPS5H100AF also contains the maximum operating junction temperature = 175°C and the thermal resistance Rth(j-l) = 16K/W. The maximum operating temperature permissible for the respective design can be calculated from the actual cooling surface of the board, the resulting thermal resistance and the power loss that occurs.
Does it answer your question?
Regards
/Peter
2025-12-14 3:42 PM
What is the minimum operating temperature?
2025-12-15 3:38 AM
The diode is specified for industrial applications with a lower limit of -40DEGC.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.