cancel
Showing results for 
Search instead for 
Did you mean: 

Help on STM32H753VIH6

jamieguinto
Associate II

Hello, 

Can someone pls help me fill this information out for STM32H753VIH6? Thank you. 

 

 

 

 

 

Model Name

Check Group

1 (注1)

2 (注2)

3 (注3)

4 (注5)

Ministerial Ordinance Article Number

第6条第一号イ

第6条第一号ロ

第6条第一号ハ

Check Items

Presence or Absence of Radiation-Hardened Design

Design Intent

Rated Operating Temperature Range (°C)

 

Whether or not compound semiconductors are used (Note 4)

Maximum Clock Frequency (Note 4) (MHz)

 

 

 

Determination Criteria

(i) Total Ionizing Dose: (Applicable) ≧ 5x10³ Gray (Si)

(ii) Dose Rate: (Applicable) ≧ 5x10⁶ Gray (Si)/s

(iii) Neutron Flux (1 MeV equivalent): (Applicable) ≧ 5x10¹³ (particles/cm²)

Is it designed for civil automobiles or railway vehicles?

(i) (Applicable) > 125°C

(ii) (Applicable) < -55°C

(iii) (Applicable) = -55 to 125°C

(Applicable) = Formed from compound semiconductors

(Applicable) > 40

(Filling Example) ABCxxxxx

No

0~85

(Compound)

30

STM32H753VIH6

 

 

 

 

 

 

 

 

 

 

 

Model Name

Check Group

1(注1)

2(注2)

3(注3)

4 (注4)

Ministerial Ordinance Article Number

第6条第一号イ

第6条第一号ロ

第6条第一号ホ(一)

 

1

2

3

4

5

 

Check Items

Presence or Absence of Radiation-Hardened Design

 

Design Intent

 

Rated Operating Temperature Range (°C)

Resolution (bit)

<10bit  resolution

8bit≦

<12bit resolution

10bit≦

<14bit resolution

12bit≦

<16bit resolution

14bit≦

 

resolution 16bit≦

 

Sampling
rate

 

Sampling
rate

 

Sampling
rate

 

Sampling
rate

 

Sampling
rate

 

Determination Criteria

(i) Total Ionizing Dose: (Applicable) ≧ 5x10³ Gray (Si)

(該)≧5x10⁶ グレイ(Si)/s

(ii) Dose Rate: (Applicable) ≧ 5x10⁶ Gray (Si)/s

(iii) Neutron Flux (1 MeV equivalent): (Applicable) ≧ 5x10¹³ (particles/cm²)

Is it designed for civil automobiles or railway vehicles?

(i) (Applicable) > 125°C

(ii) (Applicable) < -55°C

 (iii) (Applicable) = -55 to 125°C

 

>1.3

 

(Giga samples/sec)

 

>600

 

(Mega samples/sec)

 

>400

 

(Mega samples/sec)

 

>250

 

(Mega samples/sec)

 

>65

 

(Mega samples/sec)

(example)ABCxxxxx

No

0~85

10

150

STM32H753VIH6

 

 

 

 

 

 

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

As said before, I don't think this is the right place to ask for the requested information.

I recommend you to ask your local FAE/local sales.

Thank you

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
Andrew Neil
Super User

Many (most?) of those things will be in the datasheet; eg, operating temperature range, maximum frequencies.

https://www.st.com/en/microcontrollers-microprocessors/stm32h753vi.html#documentation

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
KDJEM.1
ST Employee

Hello @jamieguinto and welcome to the community;

 

Could you please look at How to write your question to maximize your chance... - STMicroelectronics Community and give more details about your issue or request.

 

Thank you.

Kaouthar 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,
I have attached the 2 documents with table and answers.
Can you pls check if all the data I input there are correct for STM32H753VIH6?

Note: The PS1 models here are all the same with STM32H753VIH6. PS1- is Audinate's product code.

Thank you.


Regards,

Jamie Guinto
Operations Compliance Admin
p: +63 9271396252
audinate.com

[Image]


PIONEERING THE FUTURE OF AV




@jamieguinto wrote:
I have attached the 2 documents with table and answers.


Nothing attached / the table contains Chinese characters .. not helpfull..

If the information is not available in the datasheet, I suggest to contact your local FAE to help you on that.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Deleted the recent post to reply correctly

Hello, 

 

I am attaching again the two files. 

Pls advise if the data here are accurate for STM32H753VIH6. 

Thank you. 

 

Jamie Guinto

Hello,

As said before, I don't think this is the right place to ask for the requested information.

I recommend you to ask your local FAE/local sales.

Thank you

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.