2026-02-08 10:17 PM - last edited on 2026-02-13 3:21 AM by Andrew Neil
Solved! Go to Solution.
2026-02-09 1:19 AM
You have already created a ticket with the internal ticket number 00254037 today, and I would ask you to wait for a response from that team. The community will not really be able to help you with your question, as it is a global forum for mutual assistance between users.
Thank you for your understanding and patience.
Regards
/Peter
2026-02-09 1:19 AM
You have already created a ticket with the internal ticket number 00254037 today, and I would ask you to wait for a response from that team. The community will not really be able to help you with your question, as it is a global forum for mutual assistance between users.
Thank you for your understanding and patience.
Regards
/Peter
2026-02-13 3:00 AM
Can I get the related information please
2026-02-13 4:15 AM
As I can see now, the OLS team has referred you to the community, which is definitely not correct. However, I can already say that an NDA (Non Disclosure Agreement) is necessary to get MTBF data, which definitely has to be handled via the OLS.
However, regarding your first question, I cannot give you any hope of obtaining efficiency curves, especially over temperature, because this depends on a great many external parameters. Among other things, the number of cells to be charged plays a very important role. The device was launched on the market back in 2010, so the probability of such a data sheet supplement is virtually zero.
Regards
/Peter
2026-03-19 10:46 PM
Can you atleast provide with the junction to case thermal resistance (Rthjc) for the IC.
Thanks.
2026-03-20 3:32 AM - edited 2026-03-20 5:31 AM
Actually, this does not directly relate to the original topic and would require a separate thread. Nevertheless, I will briefly address your new question:
Because for a small plastic package like TSSOP‑8 without exposed pad, the heat path to the ambient is dominated by junction > leadframe > pins > PCB > ambient, not by junction > case (top). In that situation Rthjc (junction-case, usually to the top surface) is poorly defined, not very useful for real applications and easily misleading.
ST therefore specifies only Rthj-ambient, measured on a standard PCB, because this reflects the realistic use case: the part soldered on a board where the PCB copper does most of the cooling. The value for Rthja is specified in the data sheet and is 135K/W.
Hope that answers your additional question?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.