2026-05-01 12:59 PM
Hello,
For the ASM330LHH, it's not clear which registers are covered by the BDU setting. Although the datasheet and application notes list some registers that are covered, they are presented more as examples than an exhaustive list.
In my testing, it appears the BDU register doesn't protect the temperature (non-FIFO) registers at all. With BDU enabled, I would still get ~1 degC temperature spikes when the sensor was operating at the rollover boundary (LSB near 0x00 or near 0xFF), due to the slight time skew between the two registers. I was able to work around this by using the FIFO.
I also need to be able to sample the TIMESTAMP registers (TIMESTAMP1, TIMESTAMP2, TIMESTAMP3, TIMESTAMP4), from outside of the FIFO. This is important because I need to periodically correlate the ASM330LHH's internal timestamp to an external time/clock; using the FIFO would introduce a large skew and a lot of complexity.
Are the timestamp registers protected by the BDU feature? Can I reliably read them consecutively, and not have to handle saturation/rollover conditions at each byte's boundary?
Thanks!
2026-05-12 9:01 AM
Well, I haven't gotten any response, so I don't know if these results are expected, but I will share my observations based upon low-level testing:
Here is some sample data proving the rollover issue affecting timestamps (this example is on the LSB; it's more difficult to catch the other bytes since they come up less frequently)...the timestamp was sampled at approx 50ms intervals; anytime the LSB is within a few ticks of rollover, there's a large delta on the order of ~6ms (on the order of ~256 ticks, with some variability due to the imprecision of task scheduling in Linux, which corresponds to full-scale of the LSB):
| timestamp | %255 | delta |
| 0x00EC2FCB | 203 | 2112 |
| 0x00EC37CF | 207 | 2052 |
| 0x00EC402D | 45 | 2142 |
| 0x00EC4860 | 96 | 2099 |
| 0x00EC5082 | 130 | 2082 |
| 0x00EC588E | 142 | 2060 |
| 0x00EC61FF | 255 | 2417 |
| 0x00EC6925 | 37 | 1830 |
| 0x00EC715D | 93 | 2104 |
| 0x00EC79AF | 175 | 2130 |
| 0x00EC81D3 | 211 | 2084 |
| 0x00EC8A01 | 1 | 2094 |
| 0x00EC9227 | 39 | 2086 |
| 0x00EC9A73 | 115 | 2124 |
| 0x00ECA272 | 114 | 2047 |
2026-05-12 10:22 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.