Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Thermal and SOA protection of L78M05AB regulator ?

I have some questions regarding the L78M05AB regulator IC.1. Could you please investigate the temperature at which this IC's the thermal protection actually activates?2. I have been informed that the thermal protection mechanism shuts down the output...

sususu_0-1777282352680.png
sususu by Associate II
  • 346 Views
  • 5 replies
  • 0 kudos

Resolved! Top marking LD59015C33R

Hello ST Team, could you please provide the marking code for LD59015C33R? Where can i find it on my own? A register to verify parts by codes would be great. Thanks Thilo Roth

Dillo by Associate
  • 158 Views
  • 2 replies
  • 1 kudos

VSTORE and LDO2 Voltage Drop When Loading STEVAL-ISV019V1

[Moderation] Separated from the previous thread, as the STEVAL-ISV019V1 is a different topic. Hi,As the questioner mentioned, the voltage measured on the STORE pin is about 2.416V. Should we charge the battery at this time? What conditions can raise ...

HUANG2 by Associate II
  • 327 Views
  • 2 replies
  • 0 kudos

Resolved! Vac sense circuit of STEVAL-7BIDIRCB

Dear ST community, I'm reviewing the Vac sense circuit of STEVAL-7BIDIRCB, where the circuit uses a resistor divider to generate a low voltage of VACN and VACL for MCU. I simulated this section of circuit in LTspice, and here is my result : My Vac in...

Saeid_2-1775942241126.png Saeid_3-1775942377861.png
Saeid by Associate III
  • 415 Views
  • 6 replies
  • 0 kudos

How energy flows in STEVAL-HARVEST1

Are there any more resources to understand how to use STEVAL-HARVEST1, how does the energy flow from super capacitors to the MCU and also the back up capacitors. I feel few things are missing the schematic and the user guide. I want to first implemen...

image.png
SaiVenkat by Associate II
  • 1032 Views
  • 15 replies
  • 10 kudos

Resolved! STSPIN840 Setting overcurrent values

Is the overcurrent protection set to 3A on the STSPIN840? If so, is there a way to change the trip value of the overcurrent protection to better align with its application? I want to change it so that the overcurrent trips at 1A. Thank you!

mnguyen1 by Associate
  • 185 Views
  • 1 replies
  • 0 kudos

Resolved! How to set STUSB4710 PDO profiles

Hi, I am designing a 25W power supply for the raspberry pi 5 for my battery powered project. The buck regulator I am using has a fixed 5V output and I want to use the STUSB4710 to offer 5V 5A to the Pi. How can I program the registers to do so via I2...

CMaker by Associate II
  • 784 Views
  • 7 replies
  • 3 kudos

STUSB4710 PD-Source Configuration Without Feedback

Hello,I am using the STUSB4710 as a PD-Source in my project and have a few questions regarding its configuration. In my setup, I have not utilized the feedback configuration. Instead, I am connecting the PDO outputs of the STUSB4710 to a microcontrol...

AHammoud by Associate
  • 958 Views
  • 1 replies
  • 0 kudos

Resolved! L9961 Cell voltages deviate during discharge

Hello, we are having an issue where our cell voltage readings are drifting when discharging. When there is no current, the voltages all read correctly. However, during discharge, we see that cell 5 and cell 1 have lower voltage readings by about 150m...

jondobrinc_0-1777677662697.png jondobrinc_1-1777677981935.png

Resolved! STTH10002's Humidity working range

Hello to all, I am looking for the min-max humidity working ranges of the STTH10002TV1 diode (in %) as I can't find it in the product specification.Is there a general value for all the ST's diodes? If so, where can I find it ? Thank you for your time...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.