Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MOSFET failure & protection

A P-channel MOSFET is currently used for switching the solenoid.Case 1:Is it possible for the MOSFET to fail?Case 2:If the MOSFET fails, will it become an open circuit or a short circuit?Case 3:If the MOSFET fails in short-circuit condition, how can ...

jalathar by Associate II
  • 452 Views
  • 16 replies
  • 3 kudos

Resolved! VNF1048 eFuse: protection against motor back-emf

在实际的汽车电子电路中,我们遇到一个问题,用efuse (VNF1048)去驱动电机,电机端会存在反向电动势,VNF1048驱动的外部的单NMOS无法做到防反功能,我们在实际电路上增加了一个NMOS,可以达到防反的目的(在efuse关闭外面NMOS时),想请教这样做有什么风险,在贵司规格书中未提及此种应用方案。 电路如如下: Google translation: In practical automotive electronic circuits, we encountered a prob...

ScreenShot_2026-05-26_190244_736.png
neo_liu by Associate II
  • 193 Views
  • 5 replies
  • 2 kudos

Resolved! STPD01 and its I2C addresses

Hi all,Hoping this is this right subsection to post the following question...I'm reading the STPD01 datasheet and it states its available I2C addresses : 4, 5, 6, and 7.Reading to general I2C documentation, it seems that these addresses are reserved ...

fabr by Associate II
  • 390 Views
  • 6 replies
  • 1 kudos

KF50BD-TR wrong pin 1 marker?

KF50BD-TR The goods have a pin indicator,but it is not shown in the datasheet .Please check attached photos.Is the product with pin indicator original?  

KF50BD-TR.png KF50BD-TR datasheet.png
DD2026 by Associate
  • 184 Views
  • 3 replies
  • 1 kudos

Resolved! STM6905 RST output

The STM6905 datasheet says in Table 2 that there is an internal 10k pull-up on RST#, which seems wrong since that's an open-drain output. Then in Section 2.6 and in Section 3 it says that an external pull-up to VCC should be used.

LED2000PUR Application circuit

I am working on a LED driver design using the LED2000PUR and would like your expert review before I proceed further. Please find my schematic and design details in the attached PDF. Could anyone please confirm whether the design and component values ...

iyer_22 by Associate
  • 103 Views
  • 1 replies
  • 0 kudos

Resolved! KF50BD-TR pin 1 marker?

What does the appearance of KF50BD-TR look like ? Does it have pin 1 marker?Can you provide the relevant drawings?

DD2026 by Associate
  • 150 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.