2026-05-04 2:32 PM - last edited on 2026-05-04 11:03 PM by Peter BENSCH
Is the overcurrent protection set to 3A on the STSPIN840? If so, is there a way to change the trip value of the overcurrent protection to better align with its application? I want to change it so that the overcurrent trips at 1A. Thank you!
Solved! Go to Solution.
2026-05-04 11:10 PM
Welcome @mnguyen1, to the community!
The overcurrent protection is designed to protect the MOSFETs and has a fixed rating of typically 3A, max. 3.5A. The low-side shunts connected to SENSEA and SENSEB on each full bridge are used for the control and limiting functions.
Hope that answers your question?
Regards
/Peter
2026-05-04 11:10 PM
Welcome @mnguyen1, to the community!
The overcurrent protection is designed to protect the MOSFETs and has a fixed rating of typically 3A, max. 3.5A. The low-side shunts connected to SENSEA and SENSEB on each full bridge are used for the control and limiting functions.
Hope that answers your question?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.