MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3: What exactly does SW_RESET do?

The LSM6DS3 has two "reboot" style operations. I've read spec sheets and appnotes but can't find a clear description of one of them.BOOT (CTRL3_C bit 7) appears to freshly load the "trimming parameters", which I presume are factory values written to ...

Resolved! Movement detection with LIS2DH

Posted on January 02, 2018 at 15:59HI everybody,I'm working with the LIS2DH for a motion sensor, and I'm using the embbeded functions of motion detection for drive the state machine of my MCU.The operation is simple, but I have some trouble with the...

How to change working modes of VL53l0X at runtime

I am using ST s API(VL53L0X TOF Sensor) and i have a doubt regarding the change in ranging modes at run time,For my application i want the sensor to work in HIGH ACCURACY mode first and after a time it has to work on FAST MODE and again back to HIGH ...

sp ra by Associate
  • 4158 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSOX And STM32cube

Hi,​I am using LSM6DSOX and ProfiMEMS​ board . I have created my modelm based on WEKA(decision tree) and I tested it in Unico v.8 and it worked.Now the question is how can I use my final model(the model which I loaded in MLC)​ in STM32cube? How is th...

spark by Associate II
  • 2362 Views
  • 3 replies
  • 0 kudos

Is it possible to access data of only one SPAD of the VL53L1X ?

Hi everyone,For a project I need to know if i can access the data of only one SPAD and not the data of the entire array.I need to detect with precision the position of some objects and I'm wondering if that is possible with the VL53L1X. My idea is (i...

MF by Associate
  • 1527 Views
  • 2 replies
  • 0 kudos

Accelerometer with higher operating temperature range?

Hi,I am using the accelerometer IIS2DLPTR and i saw in the datasheet that the maximum operation temperature is 85°C. Is there an accelerometer that has the same features that the one I am using but that has a higher maximum operation temperature?Best...

VGuer by Associate II
  • 2170 Views
  • 4 replies
  • 0 kudos

MotionAW does not leave MAW_STATIONARY

Hi,​Im trying to evaluate MotionAW on a BlueCoin dev kit. After a few seconds MotionAW_Update returns AMW_STATIONARY (before that it returns MAW_NOACTIVITY), and after that the activity doesnt seem to change. What am I doing wrong?For all I can see t...

HSmed by Associate
  • 841 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.