MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L1X RangeStatus No Update problem

Hi!I want use an VL53L1X sensor for our project. I "ported" to original ST api to TI chip and TIRTOS. But I cant measure any distance. Now I just want to try the sensor, so I using "polling" method. But when I call a GetMeasurementDataReady function...

RSzil by Associate
  • 2118 Views
  • 2 replies
  • 0 kudos

VL53L0X - how to run on stm ?

Recently I've bought vl53l0x sensors and I'm struggling 2 weeks to run it on my stm. I've bought pololu sensor and i want to connect it to Nucleo board. There is no explanation how to achieve this. There are only tutorials for specific boards and boa...

DGo�? by Associate
  • 1097 Views
  • 1 replies
  • 1 kudos

HTS221 blocks SDA line

I tried to connect the HTS221 to the ATtiny816 via the I2C bus. The data availability survey was conducted 2 times per second:if ((HTS221_GetCTRL_REG2() == 0) && ((HTS221_GetStatus() & 0x03) == 0x03)) {         HTS221_GetData(&HTS221_Rx_buf); ...

Lehman by Associate II
  • 1882 Views
  • 4 replies
  • 0 kudos

LIS331HH Frequency Response and Max acceleration detection Question

What is linearity with frequency like? I guess the sensor has a roll off at some frequency due to its mechanical characteristics?The block diagram suggests no analogue filter between the mux and A/D. How does the system deal in practice with vibratio...

JLitt by Associate II
  • 1222 Views
  • 1 replies
  • 0 kudos

LSM6DS3: DRDY stops driving INT1

Sorry for all the postings, but we're under a deadline and really struggling with the reliability of the LSM6DS3.Here's another of the strange things we're seeing on the LSM6DS3: It just stops driving DRDY on INT1. Since our present design relies on ...

IIS2DH Reset

I have an issue where the IIS2DH accelerometer gets into a state where I get no output form the axis registers. How can the device be reset without removing power? The IIS3DSH used to have a register that could be toggled for a hard reset. The IIS2DH...

iaeinfach by Associate III
  • 3739 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.