2019-04-11 10:07 AM
I would like to build a low-cost smart PH probe that can transmit water PH information. I would like to know the best options for sensors with this capability.
2019-04-11 11:33 AM
pH electrodes are pretty much just "wet cell" batteries, usually made of a thin film of a proprietary chemical deposited on glass or ceramic material. They output a small voltage that varies with the activity of a specific ion (H+ in the case of water). A very high-impedance amplifier would be able to convert the output of an electrode to an impedance and level compatible with a common ADC. Electrodes are made for immersion and also to be inserted into a pipeline, for example to monitor wastewater discharge leaving a plant. They usually have a BNC or similar two-conductor connector.
2019-04-11 12:19 PM
Check mikroelectronika click boards, there maybe one that measures PH.
These boards are supported by the STMod+ connector and Fanout board on some new STM32 discovery boards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.