| Subject | Author | Posted | |
|---|---|---|---|
|
I have been analyzing the behavior of the gyroscope thoroughly in order to quantify its drift. I di...
| 2026-06-07 11:06 PM | ||
|
This is a comment it is not a question. The older the mems sensor in acceleration the mor...
| 2026-06-06 7:45 AM | ||
|
LSM6DSM setting: acc/gyro/fifo ODR 208hz, timer resolution 25us, FIFO continous mode # 1. Enable B...
| 2026-06-05 1:39 AM | ||
|
Hello, We are evaluating the LSM6DSV16BX and LSM6DSV16X for a wearable device attached to the neck...
| 2026-06-02 9:45 AM | ||
|
Hello, I am currently using the IIS2MDC in my design with the following configuration: ...
| 2026-05-18 2:06 AM | ||
|
We are currently working with the LIS2HH12TR accelerometer on our Smarttrak board, using an STM32U5...
| 2026-05-07 5:31 AM | ||
|
I test the LSM6DSOW I3C IBI interrupt, I set the accelerometer FIFO mode, and FIFO full, the interr...
| 2026-05-07 1:42 AM | ||
|
A minimal example of wake-on-motion detection and inertial data logging based on the LIS2DW12 3-axi...
| 2026-05-06 10:03 AM | ||
|
I am using MEMS Studio (v2.3.1) with ST1VAFE3BX to train an MLC model using AFS (Automatic Filter &...
| 2026-05-05 6:36 AM | ||
|
Hey, I am using MotionFx 9D, and it works pretty well, except in one case: when a fast movement is...
| 2026-05-04 10:50 AM | ||
|
We have been using the ST MP23DB01HP microphone to measure the shockwave signature of assault rifle...
| 2026-05-03 11:40 PM | ||
|
We had three Sensor TileBox units. In an interesting morning of work, I got the one I have in the U...
| 2026-05-02 1:10 PM | ||
|
Hello, I know there are already other threads on this topic, but none of the replies have convin...
| 2026-04-30 3:26 AM | ||
|
Hello, I intend to put LIS3DH and LSM6DSV32X on same SPI bus and use different CS lines to address...
| 2025-12-30 3:56 AM | ||
|
On platforms like LCSC and Mouser, an IMU labeled "LSM6DSVQTR" is listed separately from the LSM6DS...
| 2025-12-26 3:01 PM | ||
|
Now I am working on my own project which involve with detecting the pattern of hand gestures using ...
| 2025-12-11 6:40 PM | ||
|
We have integrated LSM6DSV16X (IMU) and ISM303DAC (magnetometer) on Android 10 running on the NX...
| 2025-11-19 5:28 AM | ||
|
Dear ST, I am working with the STHS34PF80 PIR sensor on an i.MX8MP platform, using the upstream-st...
| 2025-09-18 2:27 AM | ||
|
I am using the MLC of the LSM6DSOX along with the Nucleo-L432KC. I am using the .h file generated f...
| 2025-09-10 8:05 AM | ||
|
Hey ST Community, I'm currently trying out the CCA02M2 MEMS microphone board on a NUCLEO-L476RG, u...
| 2025-08-18 11:55 PM |