2019-01-08 10:45 PM
I am using ST s API(VL53L0X TOF Sensor) and i have a doubt regarding the change in ranging modes at run time,For my application i want the sensor to work in HIGH ACCURACY mode first and after a time it has to work on FAST MODE and again back to HIGH ACCURACY mode.Is it possible ?? if yes how can i implement it on the application
Thank you
2019-04-11 4:17 PM
The only real difference between high-speed and high-accuracy is the timing budget.
Just try changing that, knowing the time will not take effect until the next range.
Technically you really should do a stop, change the timing budget and start again, but the kludge should work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.