Resolved! Markings on IIS2DLPC
Hi,I see the following markings on IIS2DLPC.1) Dot - to identify the correct orientation of sensor2) 2D code - could be for traceability3 a letter "T"What does this letter "T" mean?Thank you!
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi,I see the following markings on IIS2DLPC.1) Dot - to identify the correct orientation of sensor2) 2D code - could be for traceability3 a letter "T"What does this letter "T" mean?Thank you!
Hi All, I am working on a design that has been working for years. Now we wanted to design a revision of the PCB with the LSM6DS3TR but sadly it became obsolete and I can't find it back on the website of ST.Could the LSM6DS3TR-C be a Drop-In-Replace...
I am having STEVAL-STWINKT1 to be interfaced on USB channel for ST MEMS PC application.I have flashed DATALOG2_Release.bin in eval kit.I can get the ST MEMS PC Application showing the vibration sensor analysis graph. See attached.However, the issue I...
Hello ST Team,I am curious to know how LSM6DSV32X Accelerometers sensor communication takes place.So, basically what I am trying to understand here is when Master assigns some dynamic address to LSM6DSV32X Accelerometers sensor, then where exactly th...
Hello ST team,I’m currently developing on the STEVAL-PROTEUS1 platform and encountered an issue when transitioning from the application firmware to the bootloader.Specifically, after executing a jump from the application to the bootloader (located at...
Good morning, I am programming a SensorTile using the STEVAL-STLKT01V1 expansion kit, and when I flash the program to the device, I encounter the following error:Break at address "0x8000270" with no debug information available, or outside of program ...
我想使用 LIS12DW12 来准确测试环境温度。我应该用什么方法校准芯片的准对,否则这个芯片不能准确测量温度?有没有关于他的实验错误的数据?Google translation:I want to use LIS12DW12 to accurately test the ambient temperature. How should I calibrate the chip, otherwise the chip cannot accurately measure the temperatur...
Hi,We are using your part# LSM6DSVTR ,Can you please advise for top marking.ThanksJay Trivedi
Hi, I am trying to create test the STEVAL-MKI194V1 for a test vehicle, which has LSM6DSR. However, I do not get an initialization response from it using the Zephyr device tree. So, I did a test (without the DSL driver) with the spi shell which gives ...
We are using the LIS2DW12 accelerometer in our custom product. We understand that this sensor can detect movement or positioning along the X, Y, and Z axis. However, in our application, we need to detect when the device changes its orientation in ter...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.