MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS3DWB High-Rate FIFO/DMA Data Transfer on STEVAL-STWINBX1

Hi all, I’m working on a project using the STEVAL-STWINBX1, and my main goal is to use the IIS3DWB vibration sensor as a high-speed vibrometer. I’m still pretty new to embedded programming (about 2 months in), so please bear with me! Project setup so...

Taha by Associate
  • 1335 Views
  • 1 replies
  • 0 kudos

LSM6DSM high pass filter wake up interrupt

Hi,I am working on an accelerometer interrupt using the LSM6DSM. In AN4987 I found that I can configure the slope filter to use a window of WK_DUR samples that consecutively exceed WK_THS based on the given formula. I found good threshold settings fo...

Resolved! Bias stability of ISM330 and LSM6DSV

Hello,Could you provide the bias instability of ISM330DLC and LSM6DSV I could not find them in their datasheet ?Thank you by advance for your help

fgs by Associate II
  • 1266 Views
  • 2 replies
  • 0 kudos

Problem with reading X-axis data from LIS2MDL

The measurement data of LIS2MDL was read in the application. Both the Y and Z axes were normal, and their data changed with the position. However, the data of the X axis was abnormal, and its value was the same as TEMP_OUT. Moreover, it was not relat...

微信图片_20250619220720_5.png

Problem with LIS3DSH

Hello, it's code correct for  testing WHO_I_AM? LED doesn't work  #define LIS3DH_CS_LOW() HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET) #define LIS3DH_CS_HIGH() HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET) #define LIS3DH_WHO_AM_I_REG 0...

alexder by Associate II
  • 3054 Views
  • 9 replies
  • 0 kudos

Sensor hub no I2C communication using IIS2ILCX

Hello,I use the STEVAL-MKI209V1K with the IIS2ILCX sensor. I am trying to get the IIS2ILCX communicating with a second IIS2ILCX via sensor hub. The master sensor is connected to my MCU via SPI. Please find my „schematic“ and the configuration code be...

KoCT by Associate II
  • 1004 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.