cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DW12 – Detecting Orientation Change in Degrees Using Interrupt

Dhruvil_bhadani
Associate

We are using the LIS2DW12 accelerometer in our custom product. We understand that this sensor can detect movement or positioning along the X, Y, and Z axis. However, in our application, we need to detect when the device changes its orientation in terms of degrees—for example, when it flips or tilts significantly from one position to another.

Can the LIS2DW12 generate an interrupt based on such orientation changes (e.g., using 6D orientation detection)? We are looking for a way to trigger events when the device is rotated beyond a certain angle.

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @Dhruvil_bhadani ,

Yes, it is possible to do that.

You can look at section 5 of AN5038

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @Dhruvil_bhadani ,

Yes, it is possible to do that.

You can look at section 5 of AN5038

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.