2025-06-10 11:30 AM
Hi,
I am trying to create test the STEVAL-MKI194V1 for a test vehicle, which has LSM6DSR. However, I do not get an initialization response from it using the Zephyr device tree. So, I did a test (without the DSL driver) with the spi shell which gives me the correct chip ID output. Is the DSL driver compatible with the DSR? OR would I need a separate driver for both ?
Thanks,
Devang
Solved! Go to Solution.
2025-06-12 3:01 AM
Hi @devangs33 ,
You should use the LSM6DSR driver.
2025-06-12 3:01 AM
Hi @devangs33 ,
You should use the LSM6DSR driver.
2025-06-13 1:36 PM
Hi @devangs33
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.