2025-06-23 3:39 AM - last edited on 2025-06-23 4:09 AM by Peter BENSCH
Hi All,
I am working on a design that has been working for years.
Now we wanted to design a revision of the PCB with the LSM6DS3TR but sadly it became obsolete and I can't find it back on the website of ST.
Could the LSM6DS3TR-C be a Drop-In-Replacement for this part or another type?
Thanks in advance & kind regards,
Solved! Go to Solution.
2025-06-23 4:33 AM
The LSM6DS3TR-C is a drop-in replacement for the LSM6DS3TR, but differs in several parameters and is almost the same age as the LSM6DS3TR, so I can't recommend it as a replacement. It is also questionable whether the LSM6DS3TR-C is available in some regions of the world.
Instead, you can take a look at the LSM6DSO, which is also pin-compatible, but has a heavily modified register set, which is why the software has to be changed for it.
Hope that helps?
Regards
/Peter
2025-06-23 4:33 AM
The LSM6DS3TR-C is a drop-in replacement for the LSM6DS3TR, but differs in several parameters and is almost the same age as the LSM6DS3TR, so I can't recommend it as a replacement. It is also questionable whether the LSM6DS3TR-C is available in some regions of the world.
Instead, you can take a look at the LSM6DSO, which is also pin-compatible, but has a heavily modified register set, which is why the software has to be changed for it.
Hope that helps?
Regards
/Peter
2025-06-23 11:49 AM
LSM6DS3TR is a good choice for designing with it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.