MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MEMS Studio MLC Debug tab not available (Version 2.2.0)

I am currently trying to build a motion detector like application using a LSM6DSV80x and it's MLC in combination with MEMS Studio (fw 2.2.0). To do so, I use the standard DataLogExtended firmware on a NUCLEO-F401RE and can successfully log and visual...

tizdipietro_0-1764837233564.png

Steval Drone 02 problems

I recently purchased a mini drone set (Steval Drone 02 & Steval FCU001/V2) and encountered several issues after mounting and starting up the FCU.I would like to share these problems in the hope of finding a solution. Firstly, during indoor flight, af...

FCEDC by Associate II
  • 717 Views
  • 2 replies
  • 0 kudos

lsm6dsv calibration

Greetings,we are working on to evaluate the data given in lsm6dsv datasheet ,we want to verify the sensitivity and rest of the parameters,could you please provide us the test setup/suitable test rig details with which we can test the sensor...Thank y...

Tilt angle on a bicycle using ISM330BX

I'm using an IMU ISM330BX on my electric bicycle, and I want to detect while I'm cycling, if I'm ascending or descending a climb, and then calculate which is the angle in degrees or percentage of the slope. For this I'm using Sensor Fusion Function S...

Captura de pantalla 2025-11-19 163025.png

LPS25HP pressure sensor accuracy doesn't meet?

I am using STEVAL-MKI142V1 to read the barometric pressure by the LPS25HB MEMS sensor via SPI.The reading pressure always has a 3-4 hpa deviation or offset from the real value. (read by reference device)The RPDS registers already have values and not ...

rasemf by Associate
  • 568 Views
  • 1 replies
  • 0 kudos

LPS22HH DCR value is 0x00

I got the DCR form LPS22HH value is 0x00, but the BCR and TPID value all matched the datasheet except the DCR, and the waveforms as follow: Based on the feature showed in LPS22HH datasheet, the DCR should be 0x62but according to the DCR table (detail...

Frankly_0-1758178517338.png Frankly_1-1758178612419.png Frankly_2-1758178667739.png
Frankly by Associate II
  • 1241 Views
  • 4 replies
  • 0 kudos

Resolved! IMU Modules - Ceramic Packages

Hi,   This webpage suggests that STM can offer ceramic packages for their IMU modules. How would I go about requesting or getting a quote for a ceramic package version of any particular IMU module? thanks   

Dude by Associate III
  • 719 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.