MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ASM330LHHX : RES pin

Hi What is the function of the RES pins on the ASM330LHHX?The datasheet indicates: “Connect to VDDIO or GND.”Is there a preferred connection?Can I add a 4.7 kΩ pull-up or pull-down resistor?BR

Resolved! lsm6dsl FIFO DATA misaligned.

hi,     we use one LSM6DSL sensor to read 3 axis acc FIFO data each second, but after some times, the FIFO out data become misaligned. the sensor setting is below:XL_ODR_26HZGyro disabled.FIFO ODR = 26HzFIFO threshold (water mark) = 128No decimationB...

cdong by Associate II
  • 2783 Views
  • 7 replies
  • 1 kudos

LSM6DSOX: How to set multiple decision tree checking in FSM

Now I am working on my own project which involve with detecting the pattern of hand gestures using LSM6DSOX. I planned to use decision tree to detect each gesture and use FSM to detect the sequence of gestures and send the interrupt signal.Now the pr...

LCMGCD by Associate
  • 752 Views
  • 0 replies
  • 0 kudos

Resolved! ISM330DLC and IIS2MDC Chip Markings

Hello,I can't find reference to the expected chip markings for the ISM330DLC and IIS2MDC in their respective datasheets. My PCB assembler is requesting this information to validate the components.Are these the correct markings?ISM330DLC: SY 203IIS2MD...

Resolved! LSM6DSR RMS Noise

Hi,We are evaluating the LSM6DSR's noise floor for a specific use case. Based from the datasheet the noise is 60ug/sqrt(hz). So calculating the RMS noise at 208Hz should result to 0.00062 m/s^2 right? However, we are getting measured RMS values aroun...

adrianT by Associate II
  • 728 Views
  • 1 replies
  • 1 kudos

How to set high-g threshold for LSM6DSV320X

Hi,We are using LSM6DSV320X for our product and want to generate interrupt when high-g is detected. In which register do we need to set the threshold so that the interrupt is generated at or above that value.

Muffss18 by Associate
  • 509 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.