2025-12-04 12:38 AM - edited 2025-12-04 12:40 AM
I am currently trying to build a motion detector like application using a LSM6DSV80x and it's MLC in combination with MEMS Studio (fw 2.2.0). To do so, I use the standard DataLogExtended firmware on a NUCLEO-F401RE and can successfully log and visualise data in MEMS-Studio. The MLC training can also be done successfully, and I can flash the MLC from MEMS Studio as well as use the Decision Tree Output Viewer.
But then, when I want to tweak the parameters or understand what is going on, I am missing the MLC Debug Tab in MEMS Studio (as referred to in UM3233 (MLC section) completely and cannot test on already recorded data (see picture attached).
So where can I find the Debug MLC Tab in MEMS Studio 2.2.0? If it was removed, which is the last MEMS Studio version that supports it?
(Tested both on Mac and Windows -> same issue)
Solved! Go to Solution.
2025-12-04 1:49 AM
Hi @tizdipietro ,
MLC debug is currently available only on ProfiMEMS.
2025-12-04 1:49 AM
Hi @tizdipietro ,
MLC debug is currently available only on ProfiMEMS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.