Resolved! ISM330DLC measurement units
What are the units of the ISM330DLC reported values? SpecificallyOUTn_G to units of acceleration (g)?OUTn_XL to units of angular velocity (°/s)?I couldn't find this in your docs, may have missed it
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
What are the units of the ISM330DLC reported values? SpecificallyOUTn_G to units of acceleration (g)?OUTn_XL to units of angular velocity (°/s)?I couldn't find this in your docs, may have missed it
but i am not able to read the data in slave module, how to connect this with the host and camera module processor and read the data, is there any settings have to be mentioned.? if any one information about this it will be helpful.
Hi all,I'm working with LSM6DSOX and I managed to get the accelerometer and gyroscope data from the output registers, but the numbers don't seem to be meaningful, how do I convert the raw data to g?
Hello, I am using ST’s LSM6DSOW sensor for the Step Counting of my project that’s a Wristband. The device is worn on the user's wrist. The settings that I am using for the Pedometer are as follows:Enabling the Pedometer Algorithm: PEDO_EN = 1 Enablin...
I have an LIS3DSH securely mounted to a stationary object away from any vibration. Over the course of two and a half days, I've found the readings slowly change in value. I've tried this with multiple accelerometers (all LIS3DSH) and they always sh...
Hi, I created a SensorTile.box project in STM32CubeIDE in which I am receiving the acceleration data from the LSM6DSOX accelerometer. I would like to convert the data I receive from the sensor into the [mg] unit in the same way it is converted in the...
1. Are SPI_MISO/MOSI/CK/CS connected to STM32 MCU on the board? Logic Level 1.8V?2. Are SPI_MISO/MOSI/CK/CS_O for external connections on the board? Logic Level Vio?3. Are there a dedicated shunt for Vio connecting to 3.3V on the board?4.If a 3.3V lo...
Hello ST community. I'm currently working with a LSM6DSV in a drone application. I would like to known if there is a suggested way to cancel the gyroscope bias value?
Hello could someone explain me for the FFT LINE COMPARE that is in the ST BLE SENSOR APP for the sensortile.box what are the parameters that appear to edit? and also for the FFT COMPARE, which I understand that it will be the same and the "Name file ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.