MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Query about LSM6DSR read/write address on I2c interface

I am using LSM6DSR on I2c interface. As per datasheet when the SDO/SAO pin of the sensor is connected to ground the read/write address should be D5H/D4H but currently the read/write address is D7H/D6H. Can you please explain the reason for this? Has ...

RWasw.1 by Associate II
  • 4336 Views
  • 5 replies
  • 0 kudos

Resolved! LSM303AGR Temperature measurement??

Can anyone confirm if temperature measurement is functional on the LSM303AGR? I have everything else up and working just fine with measurements over several weeks, but temperature just return 0x00 for Hi and Lo byte. This is the third generation LSM3...

HFuxe.1 by Associate II
  • 3684 Views
  • 5 replies
  • 0 kudos

LIS2DTW12 FIFO modifying buffer size in continuous-to-FIFO mode

Hi,Is it possible to modify the amount of values that are written in the FIFO buffer after a trigger event has occurred in continuous-to-FIFO mode? Currently the device collects values in the FIFO buffer in continuous mode until a trigger event happe...

HNybl.1 by Associate
  • 1514 Views
  • 1 replies
  • 0 kudos

Resolved! I couldn't turn on the Sensortile.box

I have had testing the SensorTile.Box and today I was trying to turn it on to continue testing and dosen't work, leds didn't ligth up and the sensortilebox looks broken. I was trying to reset the sensor (plug in and plug off the battery) and press th...

SAbba.1 by Associate III
  • 1746 Views
  • 1 replies
  • 0 kudos

Problems reading Y and Z axes on the LSM9DS1 magnetometer.

Hi,While trying to calibrate the magnetometer, upon successive failures, I noticed that the values that were read for the Y and Z axes are successively repeated until a different value is read (as can be seen below). It appears that there's some kind...

0693W00000APO4WQAX.jpg
PMach.1 by Senior
  • 2910 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.