LSM6DSL FIFO threshold Interrupt
Did anyone have success configuring the LSM6DSL to use FIFO and threshold to trigger the interrupt pin?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Did anyone have success configuring the LSM6DSL to use FIFO and threshold to trigger the interrupt pin?
I just started working with the Sensotile box (STEVAL-MKSBOX1V1). I managed to upload the datalogger binary to the module (from the FP-SNS-STBOX1 function pack) and configured the sensors to acquire data via Unicleo GUI.Now I want to use a python scr...
Hi.I'm currently working on an application where I have a lis2dh12 accelerometer sharing an i2c bus with another sensor. These sensors need to be turned off by cutting off the power on the Vdd line. I'm running into issues with communicating with the...
I am interested in calibrating precisely the delay introduced by the filter chain (LPF1 and/or LPF2) of the LSMDSOX (or DSO/DSM - I presume they are the same). I have found the settling times in Table 13 of App Note AN-5272, which is a good start, bu...
I intend to use IIS3DWB accelerometer for machine vibration monitoring. In order to offset DC I intend to use HP filter ODR/800 which gives me high pass cutoff 33Hz. I wonder how to capture frequencies for a range below 33.3Hz (equipment running at 1...
Hopefully someone can assist:I am using the ST EVAL-MKSBOX1V1 (aka Sensortile Box) and trying to set up the SPBTLE-1S for use with STM32duino. I tried to follow the instructions in the STM32duino pages (here: https://github.com/stm32duino/Arduino_Cor...
I'm using a IIS328DQ on an I2C bus @400KHzEvery now and again, the part hangs up and won't talk to me. The only way out that I've found is a power reset.Attempting to follow https://community.st.com/t5/mems-sensors/if-hang-up-i2c-interface-of-the-li...
Hi everyone,I am working on a project using the SensiBLE module. It includes an STM32L476RG microcontroller and an LSM6DS3 IMU sensor. I am using I2C for communication between the two.I am trying to enable the accelerometer data-ready interrupt on IN...
Hello,I contact you because I am considering three models of MEMS microphones for an application: MP34DT05-A, IMP34DT05 and MP34DT06J.Inside the datasheet the frequency response is depicted until 10 kHz.Are these microphones suitable for an applicati...
Hi mates,Today I came with some interesting observation, I Was working with LSM6DSM sensor interface with Arduino and writing the driver code for same. I was able to achieve 4 - wire communication between Arduino and Gyro using a logic level shifter....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.