MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ASM330LHH gyroscope always sent 0 after few second

Hi I use a nucleo L432KC for a POC with an ASM330LHH. I use the internal FIFO of the ASM330 to store accelerator and gyroscope datas. I use an SPI to get datas periodically.During developpment, we used the 3.3V of the nucleo to supply the ASM330. We ...

dlb_0-1711094766109.png dlb_1-1711094795018.png
dlb by Associate II
  • 2495 Views
  • 3 replies
  • 0 kudos

Resolved! ST LIS3DH schematic review

Hello ST Community, I am currently working on a flight computer for a model rocket. It will be used together with a barometric pressure to estimate the altitude. It would be very nice if someone could review my schematic and point out any mistakes.  ...

Fazeli24_0-1711042284745.png
Fazeli24 by Associate
  • 2509 Views
  • 2 replies
  • 0 kudos

Resolved! lsm6dso 6d/4d orientation

Is it necessary to enable Free Fall detection in order to detect orientation changes? What role does Free Fall (FF) play in this context? Additionally, is there a way to set a threshold force for detecting orientation changes, such as when the IMU is...

Varsha by Associate III
  • 3415 Views
  • 5 replies
  • 1 kudos

LIS2DW12 using iio buffer, + temperature channel

Hi Problems with a iio interface and using of buffer. Goal use the iio buffer interface for accel x y, z and temperture values.    Include one Channel more for the temperature.     static const struct iio_chan_spec st_accel_12bit_channels_temp[] = {S...

KScha.3 by Associate II
  • 2139 Views
  • 3 replies
  • 0 kudos

[iis3dwb] What are the units of the BDR_XL registor?

Adjusting the register values below seems to adjust the time at which data is written to the buffer. I understood that the value is similar to Data Sampling frequency.If i set the value to 6, about 1900 data per second will be written to the buffer.I...

HKim23_0-1710207022327.png
HKim.23 by Associate III
  • 2071 Views
  • 3 replies
  • 0 kudos

asm330lhh gyroscope

hello Good Morning,       i'm working on asm330lhh imu sensor, i want to get output in angle from raw value. please give suggetion and if you source code of imu sensor so share here.  

IIS3DWB Sensor Intermediate giving Zero or Negative data

1.Sensor variant: IIS3DWB2.Communication Interface with ESP32 : SPI3. Data Reading is based on the ISR. Maximum sampling rate we are reading up to 6.7khz4.using the INT1_CTRL register for the Interrupt config  Issue Description : Based on the block s...

LIS2DH12 acceleration data not changing

Dear All, I am using the LIS2DH12 accelerometer that is incorporated within a Decawave DWM1001-DEV board. I am attempting to write a C program using the dwm.h library functions to display the acceleration values for the X, Y and Z axes via I2C consta...

GChan_02_0-1711436593131.png GChan_02_1-1711437056735.png GChan_02_2-1711437118612.png
GChan_02 by Associate
  • 2207 Views
  • 1 replies
  • 0 kudos

Query regarding IMU sensor for Golf Swing Analyses

Posted on October 23, 2015 at 08:33I am in search of 6 or 9 axis IMU mems sensor for golf swing analyses device. The device would be somewhat like  http://3bayslife.com/zone-1/ Should I go for 6 axis DOF or 9 axis DOF? Low power operation is must. A...

rahul23 by Associate
  • 2304 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.