MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DSL Custom PCB

I designed a card that uses Stm32f446 and many sensors, but although the other sensor on the I2C line works, I cannot even get an I2C OK response from the LSM6SDL. I don't think there is a mistake in the design, but I am sharing it with you anyway, t...

Resonance_0-1711045383774.png

STEVAL-STWINKT1B Altium Design Files

Hi everyone, Building a predictive maintenance device with a MEMS accelerometer. Using STEVAL-STWINKT1B as reference, but missing Altium design files. Anyone have them to share? Thanks!

dhruvit by Associate II
  • 1154 Views
  • 0 replies
  • 0 kudos

Resolved! Where is the software pack for X-NUCLEO-IKS01A2?

Last year it was in STM32CubeIDE under X-CUBE-MEMS1... now it's no longer there. The only board extensions are IKS01A3, IKS02A1 and IKS4A1. What about IKS01A2?Pietro

PB1 by Associate III
  • 1360 Views
  • 1 replies
  • 0 kudos

STHS34PF80 sensor latching to hot and cold bodies

Hi,I am working on a project to detect human presence. While testing I found that the TMOS sensor latches to a hot/cold body nearby and fails to detect humans. My measuring distance is only 6" - 10". Below is the debug of the issue I am facing with h...

sensor_latching.png
lovelesh by Associate
  • 1044 Views
  • 0 replies
  • 0 kudos

LSM6DSO32X and Changing the Full-Scale Range

I am a bit confused about changing the Gyroscope Full-Scale range during operation (dynamically).  Do I only need to change register CTRL2_G, or anything else too, to trigger a change to the Full-Scale range? What happens once I change the sensitivit...

Dude by Associate III
  • 2249 Views
  • 3 replies
  • 0 kudos

Resolved! LSM6DSO32X and INT1

If I am trying to use INT1 to indicate a "data-ready" event, does that result in a Low to High transition on the INT1 pin? Or a High to Low transition on the INT1 pin?  Does the line stay high indefinitely, until the data is read? What happens when n...

Dude by Associate III
  • 1348 Views
  • 1 replies
  • 0 kudos

LIS3DH Tilt and upside down detection

Hi all,I'm trying to use the LIS3DH to detect if the object is in a non-safe position, i.e. standing on a slope (tilted) or in the upside down position and generates an interrupt if it's one of these. Setup:Y-axis pointing downwards in the stable pos...

Resolved! LSM6DSO32X and clock sampling rate consistency

How consistent is the LSM6 sampling clock? I didn't see any details regarding clock variation at different temperatures, etc in the manual. However, I may have missed it. 

Dude by Associate III
  • 1303 Views
  • 1 replies
  • 0 kudos

Vibration speed and acceleration in time domain

There are two parameters "Speed" and "Acceleration Peak" in time domain (using MotionSP library). What condition (e.g. frequency 10Hz - 1kHz use speed and Above 1kHz use acceleration peak) will be used Speed in time domain and Acc Peak in time domai...

0693W00000ANx4hQAD.png
JTam.1 by Associate II
  • 1804 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.