2024-03-24 6:00 AM
Can LPS22HB be used to measure liquid pressure inside a miniature container with NACL solution. The sensor will be mounted at one end of the tube like container (4mm diameter). The pressure inside the liquid will keep changing due to the pressure applied from the other side of the tube. Do you think this sensor can be used in such environment ? The pressure range would be within the specified range if this sensor.
Also how do you compare LPS22HB with LPS28DFW ?
thanks
2024-03-26 2:33 AM - edited 2024-03-26 2:33 AM
Hi @sanjayd101 ,
Welcome to ST Community!
The LPS22HB is not the right choice. There are two main reasons:
LPS28DFW is right choice for the presence of gel that preserves any contamination. This device is also water proof.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.