2021-02-27 3:00 AM
I need to send the People count obtained from VL53L1X to the Server using Wifi. Does STM32 connect to Wifi or do we need an external Wifi Module for this? Also what changes have to be made in the VL53L1X code and also in which .c file of src/API folder those changes need to be implemented so that the count can be sent using HTTPS to the Server.
2021-03-18 7:43 AM
+1, i'm having the same question
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.