2026-04-07 1:12 PM
Hi everyone,
I am working with the LSM6DSM and an external LIS3MDL magnetometer and have the FIFO ODR set to 208 Hz, with no decimation configured.
I am trying to understand exactly how the FIFO handles data in the following four scenarios. Could someone clarify what happens to the samples in the FIFO for each case?
The Accelerometer or Gyroscope ODR is set higher than 208 Hz.
The Accelerometer or Gyroscope ODR is set lower than 208 Hz.
The external Magnetometer ODR is set higher than 208 Hz.
The external Magnetometer ODR is set lower than 208 Hz.
Any clear explanations on how the samples are handled (e.g., are they dropped, duplicated?) in these specific situations would be greatly appreciated.
Thanks!
Solved! Go to Solution.
2026-04-16 12:42 AM
Hi @Purvesh ,
When the sensor hub I²C read rate is higher than the external LIS3MDL ODR, the sensor hub reads the output registers at each trigger, and if the LIS3MDL has not updated its data, the same value is read and stored in the FIFO multiple times. There is no automatic duplication by the FIFO; rather, the same register value is read repeatedly until the LIS3MDL updates its output.
So,
The correct behavior is: b) The sensor hub continues to read the output registers at the trigger rate (~104 Hz in your case), but the registers are not updated until the sensor ODR, so the same data is read multiple times.
The FIFO will contain repeated samples if the sensor hub reads faster than the LIS3MDL updates its data.
2026-04-13 7:05 AM
Hi @Purvesh ,
For the LSM6DSM FIFO with an external LIS3MDL and FIFO ODR set to 208 Hz (no decimation):
2026-04-15 3:43 AM
Hi @Federica Bossi,
Just to confirm my understanding regarding the case when the sensor ODR is lower than the FIFO ODR:
In my setup:
FIFO ODR = 208 Hz
External magnetometer (LIS3MDL) ODR = 80 Hz
START_CONFIG = 0
From my logic analyzer, I observe that the sensor hub performs I²C reads at ~104 Hz.
Do you mean:
a) The sensor hub reads the external sensor only when new data is available, and the FIFO duplicates the last sample internally to match the FIFO ODR
or
b) The sensor hub continues to read the output registers at the trigger rate (~104 Hz in my case), but the registers are not updated until the sensor ODR, so the same data is read multiple times
Could you please confirm which behavior is correct in this scenario?
Thanks,
Purvesh
2026-04-16 12:42 AM
Hi @Purvesh ,
When the sensor hub I²C read rate is higher than the external LIS3MDL ODR, the sensor hub reads the output registers at each trigger, and if the LIS3MDL has not updated its data, the same value is read and stored in the FIFO multiple times. There is no automatic duplication by the FIFO; rather, the same register value is read repeatedly until the LIS3MDL updates its output.
So,
The correct behavior is: b) The sensor hub continues to read the output registers at the trigger rate (~104 Hz in your case), but the registers are not updated until the sensor ODR, so the same data is read multiple times.
The FIFO will contain repeated samples if the sensor hub reads faster than the LIS3MDL updates its data.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.