Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L3CX API With stm32l476rg error while building code

Hi folks,Im using VL53L3CX API for Stm32l476rg .Im generating code through CubeMx on keilinclude all .h & .c file from core & platform of api in inc & src folder of Project,also giving path .I got some error in Platform files & in main code .Please f...

PMOHO.1 by Associate II
  • 1392 Views
  • 1 replies
  • 0 kudos

Can the People Count data be sent from VL53L1X Sensor using Wifi ? How to integrate the Wifi Module? Also what changes have to be made in the Source Code of VL53L1X People Count for the same?

I need to send the People count obtained from VL53L1X to the Server using Wifi. Does STM32 connect to Wifi or do we need an external Wifi Module for this? Also what changes have to be made in the VL53L1X code and also in which .c file of src/API fold...

PNadar08 by Associate II
  • 1072 Views
  • 1 replies
  • 0 kudos

Question regarding VL53L1X_StopRanging()

According to the VL53L1X ULD API description when Vl53L1X_StopRanging() is called, an active ranging operation will be completed.In a practical evaluation we tried to investigate whether an interrupt could still occur after calling this function or n...

mf101 by Associate II
  • 1591 Views
  • 4 replies
  • 0 kudos

Evaluating the quality of a cover window by measuring crosstalk

In the production process of a product using the VL53L1X TOF sensor we would like to evaluate the quality of the custom assembled window. There are some mechanical tolerances and we need to ensure that the crosstalk is as low as possible. Is there a...

mf101 by Associate II
  • 1244 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1 and VL53L3CX not found in i2C Scan

Hi thereI can't find out how to connect my sensor to an arduino uno. Tried both with sample codes from SparkFun and i2C example code. It is connected in the following way:SCL -> SCLSDA -> SDAGND -> GNDVDD -> 5VI also tried with 2K ohm pull-up resisto...

0693W000008GAdCQAW.png
MTjel.1 by Associate II
  • 4922 Views
  • 9 replies
  • 0 kudos