2015-03-21 11:52 PM
I'm having problems getting the demo code to successfully RX on FlexCAN0 and then TX on FlexCAN1 (and vice versa).
canReceive() detects the new message and returns MSG_OK when using a breakpoint in canlld_receive() and stepping code. Then canTransmit() loads the TX mailbox on the other CAN with the received CAN ID and data. However, the code never seems to trigger a breakpoint when checking for MSG_OK in main(). (Demo code cut from one of the OS-less CAN demo's. Data is being received as I am successfully seeing it when copied to the periodic TX I also have running. SOmetimes the TX from the RX can be seem, but it only comes out with the periodic TX. Any ideas: - RX not returning MSG_OK (corrupted) when running in realtime? - What might delay TX until another TX? I believe double checked PADSEL, etc are OK. Note: I also found that USB only connection only puts out 3.3V on 5V. You need to use the 12V input if you are attaching CAN transceivers.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.