2025-08-08 2:32 AM - last edited on 2025-08-08 2:36 AM by Andrew Neil
Hi everyone I’m stuck and would really appreciate guidance.
What I have,
Discovery board: SPC563M-DISP (the MCU on this board needs the L9945_GUIV1.0 ELF flashed).
EVK: EVAL-L9945 (L9945 MOSFET-driver evaluation board) the L9945 evaluation package & GUI expect the discovery board MCU to be flashed with an ELF to run the demo
Questions.
1. How many/debugger types does SPC5 Studio support out of the box? Is PLS UDE the only officially supported debugger/plugin?
2. I have a PE MICRO Multilink Can I use this to flash the SPC563M? If yes what is the exact procedure (drivers, connection pins, which file formats are accepted: ELF / SREC / HEX)?
3. If using UART/FLEXCAN flashing (serial boot), what exact steps do you recommend? I’ve seen SPC5-Flasher mentioned is that the tool to use for UART/CAN (which CAN like PCAN ,Vector) flashing?
Thanks & Regards,
Arif
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.