Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

FlexCAN problems on SPC560 Discovery

Posted on March 22, 2015 at 07:52I'm having problems getting the demo code to successfully RX on FlexCAN0 and then TX on FlexCAN1 (and vice versa). canReceive() detects the new message and returns MSG_OK when using a breakpoint in canlld_receive() a...

warren2 by Associate
  • 1050 Views
  • 0 replies
  • 0 kudos

Problem with Flexcan2 and Flexcan3 in spc560b50L5

Posted on March 14, 2015 at 19:51Hi I have a 3channel can board for my project , i work with Flexcan1 with out any problem but when i want to work with Flexcan2 or 3 with a same config they did not work or any action. here is my code :automatically....

SPC560D30L3 - PWM output on channel 1

Posted on March 16, 2015 at 15:58Hello Members,I am trying to generate the PWM output on channel 1. As per my understanding, channel 0 is PA9, channel 1 is PA10 and so on. I am using the test application ''SPC560Dxx OS-Less PWM-ICU Test Application'...

ssk by Associate II
  • 3468 Views
  • 8 replies
  • 0 kudos

Bug in SPCstudio Complier or SPC MCU Family

Posted on March 16, 2015 at 19:15Hi I want to use 2 can port , i tried a lot for this issue in two MCU : SPC560B50L5 and SPC560B54L5 Both of them Have a same Response in this family when i look at the datasheet i saw a Flexcan1 have 3 CANRX pin And ...

Bug in Pinmap Wizard for SPC560B50L5

Posted on March 12, 2015 at 18:04Hi When i want to config Pin for flexcan1 in spc560b50L5 i set the pin PC10 and PC11 for TX and RX but flexcan1port not work.  (same function work for CANFlex 0) then i change the other pins in pinmap wizard like ou...

Resolved! eDMA trouble - SPC560B

Posted on March 09, 2015 at 15:01using the SPC560B-DIS board I'm having trouble with eDMA. I've got a very basic function set up to write a succession of 32bit words from one array to another using the eDMA. but it doesn't seem to ever get on to the...

patrick2 by Associate II
  • 2686 Views
  • 3 replies
  • 0 kudos

[Solved] Where to find the test application for SPC560P -DISP?

Posted on March 08, 2015 at 18:11Hi,I'm a trainee to STm. I use the SPC560P - DISP board. I've read that in the MCU flash memory there is the test application. I do not know how to run it.Can anyone help me? Thanks. #spc5 #studio #spc560p #header...

gl2 by Associate III
  • 5964 Views
  • 17 replies
  • 0 kudos

Resolved! SPC5Studio build failure

Posted on January 19, 2015 at 10:45Hello,I am trying to build a project created using SPC5Studio Wizard. The steps used are File->New->SPC5Studio Wizard. Afte this I selected SPC560D-DIS as the product line. Then selected all the drivers with OSLess...

ssk by Associate II
  • 6916 Views
  • 18 replies
  • 0 kudos

SPC56EL70L5 MCU Basic Initialization

Posted on March 01, 2015 at 00:16Dear All, Thanks for the attention. I'm working with SPC56EL70L5DISP Discovery Board using SPC5 Studio as IDE. I've never had any specific experience with such a kind of MCU indeed i'm having some trobles about how...

luigi by Associate II
  • 4180 Views
  • 9 replies
  • 0 kudos