2015-03-14 11:51 AM
Hi
I have a 3channel can board for my project , i work with Flexcan1 with out any problem but when i want to work with Flexcan2 or 3 with a same config they did not work or any action. here is my code :automatically.*/
#include''components.h''
#include''can_lld_cfg.h'' </p>
</b>
#define led1 SIU.GPDO[102].B.PDO
#define led2 SIU.GPDO[103].B.PDO
#define led3 SIU.GPDO[105].B.PDO
#define FM SIU.GPDO[69].B.PDO
#define CAN_EN SIU.GPDO[71].B.PDO
#defineASSR_EN SIU.GPDO[44].B.PDO </p>
</b>
CANTxFrame
txmsg;int
main(
void
){
componentsInit();
osalIsrEnable();
canStart(&CAND3,&can_config_canls);
SIU.
PCR
[102].
B
.
OBE
=1;SIU.
PCR
[103].
B
.
OBE
=1;SIU.
PCR
[105].
B
.
OBE
=1;SIU.
PCR
[69].
B
.
OBE
=1;SIU.
PCR
[71].
B
.
OBE
=1;SIU.
PCR
[44].
B
.
OBE
=1;SIU.
PCR
[42].
B
.
PA
=1;SIU.
PCR
[42].
B
.
OBE
=1;SIU.
PCR
[43].
B
.
IBE
=1;SIU.
PCR
[35].
B
.
PA
=0;SIU.
PCR
[35].
B
.
OBE
=1;SIU.
PCR
[95].
B
.
PA
=0;SIU.
PCR
[95].
B
.
OBE
=1;txmsg.
IDE
= CAN_IDE_STD;txmsg.
RTR
= CAN_RTR_DATA;txmsg.
LENGTH
= 8;txmsg.
data32
[0] = 0x55AA55AA;txmsg.
data32
[1] = 0x00FF00FF; ////////////////////
led1 = 1;
led2 = 1;
led3 = 1;
FM = 1;
CAN_EN=1;
ASSR_EN=1;
/* Application main loop.*/
while
(1){CAND2.flexcan->BUF[2].CS.B.IDE=0U;
CAND2.flexcan->BUF[2].CS.B.RTR=0U;
CAND2.flexcan->BUF[2].ID.B.STD_ID=0x325;
CAND2.flexcan->BUF[2].CS.B.LENGTH=7;
CAND2.flexcan->BUF[2].DATA.B[0]=0x89;
CAND2.flexcan->BUF[2].DATA.B[1]=0x66;
CAND2.flexcan->BUF[2].DATA.B[2]=0x77;
CAND2.flexcan->BUF[2].DATA.B[3]=0x44;
CAND2.flexcan->BUF[2].DATA.B[4]=0xee;
CAND2.flexcan->BUF[2].DATA.B[5]=0xaa;
CAND2.flexcan->BUF[2].DATA.B[6]=0xbb;
CAND2.flexcan->BUF[2].CS.B.CODE=0X0C;
led2 = ~led2;
osalThreadSleepMilliseconds(500);
}
}
i use the SPCStudio function's but get the same answer
Please Help About this issue
Thanks
Best Regards Vanima
2015-03-17 7:05 AM
Hello Vanima ,
Did you configure your PADSEL Correctly ? (Cf screenshot) for FlexCan2 and FlexCan3 you should configure PADSEL1 and PADSEL2 Best regards Erwan ________________ Attachments : 2015-03-17_145709.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyst&d=%2Fa%2F0X0000000bZj%2FdXeLa68hCgTfuRNFUnskok3H3ew8mWze.DB.Xmwzi0Q&asPdf=false2015-03-19 3:47 AM
Hello Erwan
I configure the PADSEL and everything is ok. Thanks a lot , it is completely solved my problem and very usefull . with Best Regards Vanima2015-03-19 9:26 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.