Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SR5E1E5 external crystal design

In the datasheet it is given at 40MHz the max C_L is 8pF (from AN6027), but the C_L in the design schema has C1 and C2 8pF(UM3305), which gives 4pF, could you suggest me with the external crystal oscillator design. And the range is from 4MHz to 40MHz...

Sreenidhi by Associate II
  • 1217 Views
  • 3 replies
  • 0 kudos

how to set SPC582B DSPI 40bit data frame size?

Dear ,       Would you teach me how to set SPC582B DSPI 40bit data frame? I use the SPC5Studio-6.0.0-Doyle, you can see my attached picture.The biggest setting of SPI frame is 32 bits.  but the data sheet says "programmable serial frame size of 4 to ...

TomJRLiu_0-1765439830260.png TomJRLiu_1-1765439934767.png
TomJRLiu by Associate
  • 426 Views
  • 0 replies
  • 0 kudos

Connection refused UDE STK on SPC574K-DISP

I am trying to connect to the SPC574K-DISP board through PLS UDE Starter kit to program but am getting a "Can't determine the default communication device! Current selection is ambiguous!" Pop up error message.I followed the Part 7 - AutoDevKit™ deta...

Resolved! is there offcial flashing tool for SR5 E line MCU?

 I can use stellar studio to flash the new software when start a debug session, but I want a separate tool to just flash the new software just like Stm32CubeProgrammer.Does Stellar team have made such tools?

feixiao by Associate II
  • 826 Views
  • 1 replies
  • 0 kudos