cancel
Showing results for 
Search instead for 
Did you mean: 

Confused About SARADC Configuration Options in SPC58ECxx RLA,

ASH2930T
Associate III

Hi everyone,

I’m working on configuring the SARADC in the SPC58ECxx using the RLA (Low-Level Drivers) tool. I want to read an analog signal on PE0 / ADC-AN11.

In the SARADC settings, I see the following options:

  • SARADC B

  • SARADC 0

  • SARADC 1

  • SARADC 3

  • SARADC 10bit modules

  • SARADC STANDBY

I’m a bit confused about which options I actually need to select. I understand that SARADC0 is the module connected to my pin, but I’m not entirely clear on the purpose of SARADC B and the other options.

Could someone clarify:

  1. What each of these options actually does.

  2. Which options I need to select if I only want to read PE0 / AN11 with SARADC0.

    ASH2930T_0-1763061097471.png

     

2 REPLIES 2
darenluie
Associate III

For reading PE0 / ADC-AN11, you only need to enable SARADC0 and the 10-bit resolution module. SARADC B and STANDBY options are for internal calibration and low-power modes, so they aren’t required for a basic single-channel read. Make sure your channel mapping in the RLA matches AN11 to SARADC0.

Giuseppe DI-GIORE
ST Employee

SARADC_B is the Supervisor SARADC able to read all analog channels. It is mainly used by safety task (redundancy).

Typical usage is:

  1. select a channel, read it SARADC_[0,1,2, ...]
  2. at the same time read the same channel using SARADC_B
  3. compare the two values

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.