Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SR5E1 figuring out current consumption

Hi,I'm trying to figure out what to expect for current consumption for the SR5E1E570C30F01X. The datasheet DS13808 - Rev 8 - November 2025 notes under "3.7 Device consumption" that "The following table [table 10] reports each single contributor facto...

VHTUL by Associate
  • 193 Views
  • 0 replies
  • 0 kudos

Resolved! Output Pins not working SPC574k

Hi,I am currently working on the SPC574k Discovery board and having issues with getting an Output on most off the pins. In my attached image configuration I only get an Output on ATOM1_0, ATOM1_1, ATOM2_1 and ATOM3_0. I use the MCS Module to generate...

Sir_Alee by Associate II
  • 1180 Views
  • 1 replies
  • 0 kudos

CAN XL for stellar SR6P3

Hello Community,I have just started working with the Stellar SR6P3 microcontroller.Do you have any CAN XL application examples or CAN XL driver examples available?I have searched within the Stellar SDK, but I could only find examples related to CAN /...

RETI by Associate
  • 380 Views
  • 1 replies
  • 0 kudos

DO NOT USE SPC5 STUDIO

For everyone who is thinking about starting a project on an SPC5x MCU: don’t. Just don’t. On paper, it looks great. Beautiful marketing slides. Pin mapping, clock tree, HW initialization… a cheap multicore debugger… everything you could ever want. Am...

MBedl.1 by Associate II
  • 838 Views
  • 2 replies
  • 1 kudos

SPC56EL70 RAM program creation and launch

Hello, recently, in attempt to create custom software for SPC56EL70 programming, I have encountered a problem to successfully launch RAM located program inside of the MCU. Discovery board is used for the test.Programming operations are commit via JTA...

Centre Aligned PWM Generation

Hi Team,We are not able to generate the Centre Aligned PWM for the SPC58NN board which has GTM Module.We are using ATOM Channel 1, where we have set the mode to SOMP and Umode as Up and Down till CN0 reaches 0.Can anyone give us the baremetal code wh...

SPC56 debug with pemicro

Hi, I am trying to debug a program running on a SPC56EL MCU, but can not find the device on the list in the debug configuration tabhow can I add SPC devices to the list?

AvitalNetzer_0-1766038103361.png

SPC58EG Checker Core

Hello, does the SPC58EG80E5xxCxx variant have the checker core feature for core 0 or is the checker core unique to the ASIL-D variant such as SPC58EG80E5xxHxx? 

nullptr by Associate II
  • 1191 Views
  • 3 replies
  • 1 kudos

startup mechanism of SPC58NNx

With the MCU enable BAF and Core0 / 1 /2 reset vectors are place at 0xFC0008 / 0xFC0004 / 0xFC000C, my question is how the 3 reset vector be called during power on? just be called one by one? the reference manual doesn't give clearly description; thi...

Long1 by Associate
  • 2087 Views
  • 3 replies
  • 0 kudos