cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5 Flash Programmer 2.8.1 – cannot connect to SPC560B64 via UART (works in 2.7.9)

mchodk
Associate

Hello,

I am facing a connection issue with SPC5 Flash Programmer version 2.8.1 when using UART communication with SPC560B64.

Setup:
Target MCU: SPC560B64
External crystal: 8 MHz
Interface: UCUART::HybridCom/7/UART
Same hardware setup as previously used successfully

SPC5 Flash Programmer v2.7.9 works correctly on an older PC, v2.8.1 (and newer) fails to connect.
The software stays in “Connection phase starting” and continuously retries, the UART interface LED does not blink. No connection is established.

Same SPC560B64 device, same UART interface and wiring

Are there any required driver updates, configuration changes, or compatibility notes for newer versions?

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.