Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC58: SPI2 with two chip selects

Hi.I want to use DPI2 located at pins 66 (miso), 68 (mosi) and 112 (clock) to control two different SPI slave devices. Pin 57 (CS0) and pin 64 (CS2) are wired to the respective chip selects.Then I used the wizards to generate application code for SPI...

SMay by Associate II
  • 5464 Views
  • 11 replies
  • 0 kudos

Resolved! how to select and unselect DSPI slave select lines

while using the DSPI example in spc58ec_disp , i couldn't see that the "spi_lld_select" and "spi_lld_unselect " functions usage to control the slave pin. and it didn't had any effect while i used the functions. how could i use the functions to contr...

Couldn't monitor voltage in eval l9963.

Recently i bought the eval l9963 bms board from st. As i was playing with it with a 4 cell ​li-ion battery connected in series. I'm trying to monitor the battery using the STSW gui software. I connected the batteries as per the user guide connected i...

RKP.2 by Associate II
  • 2298 Views
  • 3 replies
  • 0 kudos

Resolved! SPC582B-DIS (Can't connect target!)

I have bought the SPC582B-DIS EVB from Mouser. (SPC582B-DIS STMicroelectronics | Mouser Korea, Republic of)However, this product doesn't work normally. I think there is a problem with FDTI Dirver chip as below.So, I asked Mouser for a refund. Howeve...

0693W000007EG6BQAW.png
BKim.5 by Associate II
  • 4710 Views
  • 7 replies
  • 0 kudos

SPC5 Timebase Example?

Specifically for the SPC58 -- although it looks like the 56/57 share the same registers. I've reviewed the documentation for the time base registers (TBU/TBL) and have made an attempt to enable it. Leaving the timebase clock (SEL_TBCLK) at the proces...

VMiki.1 by Associate II
  • 2046 Views
  • 3 replies
  • 0 kudos

Resolved! How to generate UART RX INTERRUPT WITH SPC58EC-DISP

Hello All,I am working on UART on SPC58EC-disp Discovery board importing and using example source code "SPC58ECxx_RLA SERIAL DMA Test Application for Discovery" in SPC5Studio. I can transmit the data but unable to receive the data by interrupt method...

Orazio by Associate II
  • 9585 Views
  • 6 replies
  • 0 kudos