Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5 Studio

Posted on December 04, 2017 at 07:31Hi, We are planning to use SPC5 Studio as IDE for SPC56xP series microcontroller.I would like to get information on the below points regarding the SPC5 Studio.1. I understood that its free trial evaluation is avai...

Resolved! How to run SPC58EC ETHERNET RMII mode

I have SPC58EC-DISP,now I use sample code(Network Gateway Test),it's MII mode and working; then,I want to use RMII mode,I set PHY MODE = RMII,it's not working, how to do it?ps:The OSC is changed to 50MHz,and SB5 Close & SB6 Open.

0693W000008w6hdQAA.jpg
SLEE.6 by Associate II
  • 7699 Views
  • 3 replies
  • 0 kudos

Resolved! DSPI configuration problem

Hello,Actually, I'm trying to make an SPI communication between SPC574S-DISP and L9960S-EVAL.I already configured all things i can for the communication and it works, but sometimes there is an error in the RX Buffer.I think that the craddle of this i...

0693W000008x3pWQAQ.jpg
Bastien1 by Associate III
  • 1422 Views
  • 1 replies
  • 0 kudos

Resolved! Need MCU with 2 CAN Transceiver and 2 Ethernet MAC

Hi,I need a MCU with 2 CAN transceiver and 2 EMAC interface for my design. I found that SPC58 series have the same. But the complete part number is not available from the site.Please help me to find out the correct part number for design with 2 CAN t...

Mom.1 by Associate II
  • 1944 Views
  • 1 replies
  • 0 kudos

Resolved! spc560b-cant jump from my bootloader to app code

hi I make my bootloader and app code.in bootloader I have assembly code for branch and in my app code i have a led.I set app.ld for bootloader to 0.00000000 and set for app code to 0x00010000 address. It cant be jumpplease help measm volatile ("e_li...

Resolved! FreeRTOS Using ADC

Hello,I'm a beginner in FreRTOSS but I've already made basics codes and tutorials. Actually, I'm trying to do two different tasks. The first one is an ADC acquisition and the second one is a printf of the ADC value.But my issue is that the ADC functi...

Bastien1 by Associate III
  • 5286 Views
  • 4 replies
  • 0 kudos

Resolved! UNABLE to install PLS UDE

i AM TRYING TO INSTALL PLS UDE uising the recommended link: http://spc5.drive.cloudforge.com/projects/spc5tools/updatesbut all i can see is the following message.ForbiddenYou don't have permission to access /projects/spc5tools/updates on this server....

0693W000004Ia8cQAC.png 0693W000004Ia8hQAC.png
VLELE.1 by Associate II
  • 4985 Views
  • 6 replies
  • 0 kudos

Resolved! Debug first project in SPC5 Studio

HelloI am new to SPC5 Studio, please guide me how I can debug my first project.I am working with SPC5 Studio ver 6.0.0. and have SPC56D_DISCOVERY Eval board. Thanks

Parth1 by Associate II
  • 4369 Views
  • 5 replies
  • 0 kudos

Resolved! Link between LIN and TERA TERM

Hello, I'm trying to develop on SPC5 Studio with the eval board SPC574S-DISP. I want to make a link between LIN and the software tera term to debug my code. I configured pins PA5 and PA6 for LIN according to the schematics. But it didn't work. Can yo...

Bastien1 by Associate III
  • 1439 Views
  • 2 replies
  • 0 kudos

Resolved! Sending float over serial communication

Hello, I'm actually trying to send data from the software Serial Port Monitoring to my dev board SPC574S-DISP.But it doesn't work. When i send a number like "3", it works.But when i try to send "3,3" or "12", the board takes only the first number "3"...

Bastien1 by Associate III
  • 1932 Views
  • 2 replies
  • 0 kudos