AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Issue with SPI between BMSCCTX and C4MINI

Hello team,I am using the GUI demo (single) for BMSCCTX and C4MINI with 4 LFP Batteries. I have followed the steps described by @ritehracingteam in this thread.After I run the program from the AutoDevKit Studio, my D9 and D2 LED are lit up and D8(Blu...

Zen432 by Associate II
  • 871 Views
  • 4 replies
  • 1 kudos

Resolved! Doutb regarding Daisy chaining BMSCCTX with BMSCCTX

Hi team,I have seen example of C4MINI1 daisy chaining BMSCCTX with BMSCC which is working fine.I have 2 BMSCCTX, so i was wondering that i can connect 2 BMSCCTX for daisy chaining with C4MINI1.But i have noticed that in the datasheet of CCTX, the dai...

Amal_V by Associate III
  • 491 Views
  • 1 replies
  • 1 kudos

Resolved! Spi not working in AEK-POW-BMSCCTX

Hi team,I am trying to run BMSCCTX using Pi as MCU. 1. I read the L9963 E and L9963 T datasheets. i found that any 8 bit message wakes up the BMS , i tried sending sample messages like 8 bit zeros and was able to turn on d2 led of bms.if the wake up ...

Amal_V by Associate III
  • 653 Views
  • 2 replies
  • 0 kudos