cancel
Showing results for 
Search instead for 
Did you mean: 

Availability of High-Level BMS APIs (AEK_POW_BMS63EN) in AutoDevKit

ASH2930T
Associate III

Hello,

In the AEK-POW-BMSCHAIN example code, I see high-level APIs like:

 
AEK_POW_BMS63EN_GetModule() AEK_POW_BMS63EN_init()

But in my AutoDevKit installation, only low-level chain APIs (AEK_POW_BMS63CHAIN_*) are available.

Could you clarify:

  1. Are the high-level AEK_POW_BMS63EN APIs included in the public AutoDevKit package?

  2. If not, are they only available via partner/NDA packages?

  3. Should regular users implement high-level functionality using only the low-level APIs?

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
Max VIZZINI
ST Employee

Hi,

No, there is no reserved code / package.

The code is available for evaluation purposes.

If you need design support to your coding, you can consult with our partner https://www.beond.net/electronics/ 

Best Regards,

AutoDevKit Team

View solution in original post

1 REPLY 1
Max VIZZINI
ST Employee

Hi,

No, there is no reserved code / package.

The code is available for evaluation purposes.

If you need design support to your coding, you can consult with our partner https://www.beond.net/electronics/ 

Best Regards,

AutoDevKit Team

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.